AnsweredAssumed Answered

compressor in ADAU1452

Question asked by mwalters on Aug 31, 2017
Latest reply on Sep 14, 2017 by TylerK

I am using Sigma Studio version 3.15.2 and ADAU1452, controlled by a microprocessor. 

 

Regarding the Standard Stereo Peak Compressor (located in the Sigma Studio toolbox as Dynamics Processors / Peak / Standard / Full Range / Standard Peak):

 

1. Is there an equivalent mono version available? 

 

2. If I want to bypass / disable the compressor (without creating a bypass signal stream), can I simply get the microprocessor to set all the points to SIGMASTUDIOTYPE_8_24_CONVERT(1)? What would I set the hold, decay & attenuation values to?

 

Regards

Mark

Outcomes