AnsweredAssumed Answered

ADV7280 - Modifying script

Question asked by JFIX on Aug 31, 2017
Latest reply on Sep 29, 2017 by Rob.Analog

I'm using the ADV7280 Evaluation Board with the "DVP Eval Latest Source 10-14-11" software.  I've modified the "Autodetect_CVBS_Single_Ended_In_Ain_1_YPrPb_Out.py" script so that the ADV7391 outputs CVBS instead of YPrPb.  I've attached my modified script.  My problem is that about 50% of the time the screen appears without color.  The status registers are as follows: Status1 = 0x0D; Status2 = 0x00; Status3 = 0x69.  If I disconnect the video source and then reconnect it the color works and Status1 changes to 0x0F.  What is wrong with my script?

Outcomes