AnsweredAssumed Answered

HMC284A Control Input Tolerances 3V ± ? Vdc

Question asked by sss on Aug 31, 2017
Latest reply on Sep 14, 2017 by s.ilke

Hi all,

 

I checked following thread,

Low control voltage operation of HMC284A

Low control voltage operation of HMC284A 

 

"The HMC284A is specified in datasheet for 5V operation.
However it can be operated with control high voltage range from 3V to 7V on which the part have already been measured during product characterization."

 

Our customer question is,
What is the control input tolerances & threshold at following each voltages.

 

From datasheet,
Vctl = 0/+5 Vdc
Control Input Tolerances are ±0.2 Vdc

 

Vctl = 0/+3 Vdc & Vctl = 0/+7 Vdc
Control Input Tolerances are ±0.2 Vdc ? threshold ?
Is it the same, Vctl = 0/+5 Vdc ?

 

Best regards,
sss

Outcomes