AnsweredAssumed Answered

AD9371 No OS code without 30.72MHz reference

Question asked by filabrasil on Aug 31, 2017
Latest reply on Sep 1, 2017 by DragosB

Hi,

I want to know how to modify the code to work without the 30.72 MHz. So far what I did is

1. modify the ad9528.c file as  mentioned in AD9371 board - AD9528_initialize() failed 

   }while((reg508 & 0x27) != 0x27);

and replace it with:

   }while((reg508 & 0x26) != 0x26);

2. set clockPll1Settings->bypassPll1 to 1 in myk_ad9528init.c

 

However, in the line

ad9528Error = AD9528_initialize(clockAD9528_device);

ad9528Error results in ADIERR_FAILED.

 

I think the code still seem to work fine but I want to make sure I am not breaking anything.

Outcomes