AnsweredAssumed Answered

What we should do for "adi_pwr_SetFreq failed" error in VendorUsbDemo_BLIP2 code ??

Question asked by gop24 on Aug 30, 2017

** I am getting the error when i run the VendorUsbDemo_BLIP2 code using CCES 2.6.0 on ADZS-BF707-BLIP2 Rev 2.0

OUTPUT : 

Loading application: "C:\Users\Synapse\cces\2.6.0\examples\bf707_blip2_1.0.0\Vendor USB Demo\Debug\VendorUsbDemo_BLIP2.dxe"
Load complete.

adi_pwr_SetFreq failed

Core clock: 384000000 Hz
System clock: 192000000 Hz
System clock 0: 96000000 Hz
System clock 1: 192000000 Hz

Waiting for Command from Host

 

* *When i changed      #define SYSCLK_MAX (216 * MHZTOHZ)  to #define SYSCLK_MAX (192 * MHZTOHZ)
i.e when it is reduced it will not show you any error and i am not able to see the output on the command prompt when i give commands .

 

OUTPUT:

Loading application: "C:\Users\Synapse\cces\2.6.0\examples\bf707_blip2_1.0.0\Vendor USB Demo\Debug\VendorUsbDemo_BLIP2.dxe"
Load complete.

Core clock: 384000000 Hz
System clock: 192000000 Hz
System clock 0: 96000000 Hz
System clock 1: 192000000 Hz

Waiting for Command from Host

 

** Is that ok to change SYSCLK_MAX to get the output ,if it is then what value we need to give to get the output.

    Can you please suggest if there is something else to be done other than changing SYSCLK_MAX to get output when command is given .

Outcomes