AnsweredAssumed Answered

ADAU1466 compiler error?

Question asked by ChristianH on Aug 30, 2017
Latest reply on Jul 31, 2018 by edarring

Hi,

 

I'm just playing around using the Sigma Studio V3.15 Beta 2 and a ADAU1466 chip.

I'm using some delays in my design but the compiler issues an error message if I try to use more than 32K per data memory.

 

The compiler_output.log says

##### Summary #####
DM0 RAM used:       32016    (of 40960)
DM1 RAM used:       29741    (of 40960)
PM  RAM used(Data): 00000    (of 24576)
PM  RAM used(Inst): 00324    (of 24576) 246 instructions (32bit: 168  64bit: 78)
Total PM used:      00324    (of 24576)

 

If I try to add another delay block that exceeds 32K in one of the data memories I get an error message:

"Assembler Error. Object reference not set to an instance of an object."

 

What could be the problem here?

 

Regards

Christian

Outcomes