AnsweredAssumed Answered

Can i program HSC-ADC-EVALEZ on a demo code/template?

Question asked by fineconcerto@neusoft.com on Aug 29, 2017
Latest reply on Sep 14, 2017 by DougI

Hello,

 

I have a question regarding the HSC-ADC-EVALEZ and AD9656.

Currently I can use Visual Analog to capture RF signal center frequency @~ 64Mhz with AD9656, through HSC-ADC-EVALEZ. However, with Visual Analog, I can only use the mouser to click start acquisition button( which should be implemented via SPI ).

 

I would like to capture a RF frequency sweep signal( RF duration~ 1ms, frequency span~=800Khz, center frequency=64Mhz). And I would like a gated signal to trigger the acquisition window. With gated signal, I can align the TX frequency sweep signal exactly with my acquisition window.

 

I am thinking if ADI already offered some demo code of the HSC-ADC-EVALEZ. If so it must be easier for me to customize( maybe I can connect one of SMA connector to a gated TTL signal) while I do not need to program the Virtex-6 from the beginning.

 

Best regards,

Tangji

Outcomes