AnsweredAssumed Answered

iSensor ADISUSBZ with ADIS16405BMLZ imu

Question asked by guglielmo.cervettini on Aug 28, 2017
Latest reply on Aug 28, 2017 by NevadaMark

Hi everybody! Here is my question:

i have to use the iSensor ADISUSBZ pc-usb evaluation system with the ADIS16405BMLZ imu on a windows 7 pc (64bit).

I've installed Adis16405_Eval_3 and GIVEIO on the pc but when i connect the board with usb cable the usb drivers installation has issues (doesn't start automatically).

Do i need some installation cd? Can i do the driver installation if i don't have any cd?

thanks everybody!

Attachments

Outcomes