AnsweredAssumed Answered

EVAL-ADV7613FEBZ

Question asked by gman99 on Aug 24, 2017
Latest reply on Aug 29, 2017 by JeyasudhaMuthuPerumal

(new thread spawned off this discussion as requested)


We have the EVAL-ADV7613FEBZ eval board and we're trying to confirm it works in HDMI passthrough mode (from a laptop). As suggested in the quick setup guide (from the other thread), JP3, 4 & 5 are disconnected, XRC 2p0RC2 is installed and I ran the 2_03_HDMI_Input_LVDS_Output_Port_A_and_B script after confirming connections were fine and the SDP drivers were working

 

I had to additionally run the EDID_Example script before my laptop recognised the external HDMI device.

I still don't see HDMI out of the board. I noticed there was an additional script titled 04_01_ADV7511_HDMI_output. I ran that script as well to no avail.

 

Is there anything else I can try. Does the onboard FPGA need to be programmed?

 

PS: Also, the user guide has a screenshot of the board selector screen where it tells you to pick the ADV7613_2 as the Rx and OUTPUT_MODULE_E as the Tx.

When I run the board selector, tx option is for the ADV7511. I assume this is because one of the script files I downloaded from the engineering zone has been updated since the Quick_Setup_Guide was  written?

 

Board Selection Screenshot

Outcomes