AnsweredAssumed Answered

using external memory

Question asked by songcomeshere on Aug 24, 2017
Latest reply on Sep 6, 2017 by Jithul_Janardhanan

Hi, I am developing a program using CCES on the platform of BF707. In order to use the external LPDDR memory, I initialized LPDDR and checked the option "use external memory(SDRAM)" in system.svc(see figure 1.jpg). Everything works well when I debugged with ICE1000. But when I burned it in the flash, the program does not run after reset. It seems that the default program entry is changed and some extra settings are needed in CCES. Is there something wrong with the settings of CCES? Thanks a lot.

check the option

Outcomes