AnsweredAssumed Answered

AD7293 Vrefout issue

Question asked by sultza on Aug 23, 2017
Latest reply on Sep 14, 2017 by valerie

Hi, I have an AD7293 with Vrefin connected to Vrefout. There is nothing else connected to these pins, except a capacitor. Vdd is at 5V. I have 3.1V on Vrefout. On Vrefad there are 0.56V.

In the AD7293 pdf, there is the following: Vrefin internally connected to Vrefout, Vrefad is half of Vrefout.

Image extracted from pdf, 6/2016—Revision A: Initial Version

On Vrefout, there should be 2.5V instead of 3.1V.

Anyone knows the cause of this?

Outcomes