AnsweredAssumed Answered

Synchronizing pulse edges with a clock signal

Question asked by jpotter0 on Aug 23, 2017
Latest reply on Aug 30, 2017 by pkern

I need to align a 3.3 V CMOS pulse with a 150 MHz clock. The pulse length is 10 usec or so. The clock amplitude is about 1.2 V, not high enough to drive 3.3 V CMOS directly. I'm looking at using an AD9513 with CMOS output to drive two cascaded 74LVC74A D flip-flops. Is there some AD device that already does this? I need a total of 4 circuits with a common clock. Thanks - Jim

Outcomes