AnsweredAssumed Answered

ADSP21489 100 lead package SPI boot?

Question asked by mhdfr86 on Aug 21, 2017
Latest reply on Aug 28, 2017 by mhdfr86

hi,

I'm evaluating the processor   

ADSP-21489  . 100 lead package.

I want to know if it supports booting from serial SPI flash memory, the one like M25Pxx.

the datasheet indicate that there is 2 booting mode, Master SPI and Slave. which a bit confusing.

also the default slave select PIN, is it the FLAG0 pin which is lead number 77 or the DPI-P05 lead number 23.(always 100 lead package).

 

thanks a lot.

Outcomes