AnsweredAssumed Answered

ADRV9371 + ZC706 using 2016_R2 boot errors: bad board or external reference clock required?

Question asked by sbt-bud on Aug 15, 2017
Latest reply on Aug 18, 2017 by sbt-bud

Errors in the boot (see badboot log attached) with the 2016_R2 image downloaded from the wiki:

ERROR: 282: MYKONOS_waitInitCals() returned an ARM error
ERROR: 257: Device not in radioOff/IDLE state. Error in MYKONOS_enableTrackingCals()
ERROR: 360: MYKONOS_waitArmCmdStatus() exited due to ARM error for the desired ARM opcode
ERROR: 144: ARM command to move to radioOn state failed.
ERROR: 360: MYKONOS_waitArmCmdStatus() exited due to ARM error for the desired ARM opcode
ERROR: 256: ARM Command Error in MYKONOS_setObsRxPathSource()

 

We have another ADRV9371 in the lab that works fine with this ZC706 (see goodboot log attached).

Do I have a bad board?

Do I need an external clock reference?

(I've pored through the forums but not come away with a definitive sense of the answer)

 

Thanks,

 

-Bud

Outcomes