AnsweredAssumed Answered

AD9361 Tx bb second filter

Question asked by Selwyn on Aug 15, 2017
Latest reply on Dec 7, 2017 by mhennerich

Hi,

 

I will like to know what is the formula to compute the resistor and capacitor value for the tx bb second filter as I could not find it in the reference manual ug570 , page 32 as well as the register map reference map ug671, page 33. I am also trying to understand the formula used for the tx bb first LPF.

 

I am currently using picozed-sdr2 platform using reference design 2016_1 as well as no-os driver 2016_r1. I am doing some simple transmission and based on my SA observation, I was unable to determine why there is a huge transition band.

 

I was trying to understand the formula stated in these 2 functions found in ad9361.c :

1) ad9361_tx_bb_second_filter :

 

       For this second bb filter , there is no formula used in register map reference map ug671, page 33 but was mentioned reference manual ug570 , page 32 that it is typically calibrated to 5 times the baseband channel bandwidth.

 

      1.1)Does the 5 times explain why inside the function it calculate the corner = BBBW * 5*pi ? How does the pi come       into the picture? Is it related to the cut-off freq : fc = 1/( 2*pi*R*C) where as R = resistor and C = capacitor ? If that is       the case, should it be 5* BBBW * 2pi ? The same concept which is implemented in ad9361_tx_bb_analog_filter       where there is a calculation of 1.6*BBBW *2*pi.

 

      1.2) And I realized there is a calculation error here.

                  It stated : corner = 15708 * (tx_bb_bw  / 10000UL);

 

      5 * pi = 15.7078 , because of the "/10000", the result should be 157080. There is a short of one '0' at the end, and       that in fact improve the transition band by a bit. Is this a typo error or meant to be?

 

2) Lastly like to ask how is the calibrated value calculated ? Like how do you determine that the first BB LPF  is 1.6 times and second BB LPF is 5 times?

Outcomes