AnsweredAssumed Answered

AD9375 IIO scope plugin not visible

Question asked by jmueller on Aug 11, 2017
Latest reply on Sep 11, 2017 by jmueller

Hi, I am currently evaluating the ADRV9375 eval board. It comes with 2 SD cards:

 

1. One for use with Windows GUI. It runs as a Linux on my ZC706. IIO scope is installed. However, it can be used to connect the Windows GUI to the AD9375. (Image name: "AD9371 Image 20161130.img")

2. One for use as standalone with the Zync ZC706. As the version shipped was outdated, I used the newest version 2016-R2. (Image name: "2016_R2-2017_06_29.img") I prepared the SD card for use with ZC706 and AD9375. IIO Scope is installed.

In both environments, if I start IIO Scope and click "connect", I can see the ADRV9375 card. However, the plugin (basic and advanced) are not displayed. Am I doing something wrong?

 

With the Windows GUI, the TRX is working.

 

Thank you very much for your help!

Outcomes