AnsweredAssumed Answered

ADAU1452 - warning (27,ExtDelay1): Preprocessor macro re-definition?

Question asked by op-electronics on Aug 10, 2017
Latest reply on Oct 2, 2017 by op-electronics

Hello,

 

i get this warning once i do the link-compile-connect or link-compile-download:

 

warning (27,ExtDelay1): Preprocessor macro re-definition of 'PIN_DRIVE_MAX_SPEED_NO_PULL'with different value (3922,0)

 

The application uses Voltage Controlled SPI Delay with 23LC1024 RAM and Master Control Port SPI Interface through 25AA1024 EEPROM (which holds program memory data too). When i run the program Voltage Controlled SPI Delay stops working and passes no signal anymore while Master Control Port Interface seems to work fine.

 

If i do remove blocks for Master Control Port Interface than Voltage Controlled SPI Delay starts to work again.

 

Can you help me understand what's happening?

 

If needed i can send the program but i would prefer not to publish it here.

 

Thank you

Omar

Outcomes