AnsweredAssumed Answered

ADF4360-9 :-  cp out (pin 24) is coming like a square wave.

Question asked by sam564 on Oct 24, 2011
Latest reply on Oct 25, 2011 by rbrennan

I am using ADF4360-9 to generate 120MHz clock. Ref input is 10 MHz.

 

The circuit is working fine in two boards. But in third board it is giving some issues.

 

The CP out (pin 24) is coming like a square wave of   5Kz.

 

What could be the problem ?

 

 

Thanks and Regards,

SK.

Outcomes