AnsweredAssumed Answered

HSC-ADC-EVALDZ and AD9683-250 EVAL Board

Question asked by robinsheehy on Aug 9, 2017
Latest reply on Sep 26, 2017 by J.Harris

Hello,

 

I have been tasked with setting up and using two boards

 

   1xHSC-ADC-EVALDZ

   1xAD9683-250 EVAL Board (Only other identifying text is 08-035115 REV A, 9683CE01B)

 

I have worked through the quick start guide I have found online but I cannot seem to get the system to work as expected.

 

When I run VisualAnalog all I get is an error message at the bottom that says.

 

ADC Data Capture Error: Timed out while attempting to fill FIFO(s)

 

The boards were bought separately and I am wondering if the AD9683 I have is only compatible with the HSC-ADC-EVALEZ  Is there an easy way of determining this?

 

Sometimes when I am making changes in SPIController I get the following error messages.

 

Crtl JSLCjtx_l_cfgCmbBx02 reg value 10 not found

 or

Crtl JMCjtx_m_cfgCmbBx02 reg value 15 not found

 

I am running the following Software Versions.

 

SPIController - 4.0.11.4577

VisualAnalog - 1.9.46.16

 

Thank you  for any help you can provide.

 

Images of the two boards below.

 

AD9683 EVAL BOARD

HSC-ADC-EVALDZ Board

Outcomes