AnsweredAssumed Answered

Unable to run Image Processing Toolbox examples on ADZS-BF707 BLIP2

Question asked by heisenbug on Aug 8, 2017
Latest reply on Aug 10, 2017 by heisenbug

I tried and successfully ran the VOS/IOS examples through the ADVision Sensor Control GUI. I also successfully debugged the char_echo example.
Now, I'm trying to run the corner_detect_bf707 example located in Image Processing Toolbox RF 2.4.0 but with no luck. I've tried following the user guide. I noticed that there aren't any specific instructions for BLIP2 so I've been following instructions for ADSP-BF707. At first, I noticed that the red LED on the BLIP2 would turn on after I started debugging the program. Upon further investigation, I noticed that the program would freeze at line 1482 of adi_pwr_v2.c (WaitForLock(pDevice);) and the following error was thrown in the console:

 

A non-recoverable error or exception has occurred.
  Description:   No dispatched handler available for the specified interrupt code.
  General Type:  RunTimeError
  Specific Type: NoDispatchedHandler
  Error Message: Enabled interrupt with ID (IID) 0x0013002c raised when it has no handler registered.
  Error PC:      0x11a000c8

 


I'm using CrossCore Embedded Studio v2.6.0.0 on Windows 10 Build 15063

Outcomes