AnsweredAssumed Answered

I want to port the ML605 LVDS code to Zynq. I only want to use the LVDS data acquisition and not DMA. Please help.

Question asked by makarand.deshmukh on Aug 8, 2017
Latest reply on Aug 11, 2017 by rejeesh

I am trying to use the AD9278 with Zynq and have downloaded the reference design ML605. I can see that there's a DMA interface in the code. However, I am not able to find SPI interface for configuration, and I have implemented that. 

 

I also would like to use the LVDS data acquisition from the reference design in ZYNQ. I do not understand what sections do I have to use. Also, if the bit alignment routine is running all the time, it seems to be based on the PN sequence. For this, I think the PN sequence test would have to be enabled in the AFE. I think this is done via the PC utility, but in my case, I guess I will have to do it via the FPGA. Please help me to understand what part of the reference code I need to use.

Outcomes