AnsweredAssumed Answered

Remove unknown DC offset and Add Know DC offset to AC signal

Question asked by rajkanika on Jul 31, 2017
Latest reply on Aug 14, 2017 by rajkanika

Hello,

 

I have a pressure sensor, which has a nominal voltage output voltage of 2.0VDC from the sensor and when pressure changes, the signal changes from 2.0VDC +/0.2V DC. So there is a 2.0V DC offset and +/-0.2V if the AC signal on top of the 2.0VDC offset, the signal frequency is 0.1Hz (I have attached a picuture (originalsignal.png)).

 

I have to amplify just the AC signal on top of the 2.0VDC offset by 5 times but keep the DC offset to 2.0VDC, which i can do it by a differential amplifer by connecting the inverting pin to the signal and non inverting pin to 2.0V reference signal and add a reference voltage of 2.0VDC on the inverting pin to get  (3.0V positive peak and 1.0V negative peak with 2.0VDC offset).

 

The real issue i have is, my 2V DC offset  on top of AC signal from the sensor may change anywhere between 2V - 1.5V, because of things happening at the reference port of the pressure sensor.

 

I need to have a fixed 2.0VDC offset on the output signal and just amplify the AC signal (+/0.2V AC signal), no matter where my DC offset on the input signal  (DC offset may change from 2V DC - 1.5V DC). So i has an idea of if i can build a Differential amplifier with reference of 2.0V on the non-inverting pin, so i get the error signal (DC offset error of 0.2VDC when the offset of the sensor signal is 0.8V) and if i know what the error is, i can add it back to the signal source using Opamp Adder. But the problem is that, i will have +/-0.2V AC signal on top of 0.2V DC offset.

 

I need a constant 0.2VDC error voltage to add it back to the 1.8VDC offset +/- 0.2V AC signal, so that i can have a constant DC offset of 2.0VDC. (I have attached a LTspice simulation file for reference)

 

I have tried a high pass filter, but the problem is my roll of frequency of 0.1Hz. At this low frequency, there is a huge signal phase shift on the output signal (nature of a filter) and my design cannot afford any signal distortion or phase shift because of the application.

 

I would really appreciate your help and ideas.

 

Thanks,

Raj kenika.

Outcomes