AnsweredAssumed Answered

Error : "Failed to get CPU status after 4 retries".

Question asked by RMS-69 on Jul 31, 2017
Latest reply on Aug 3, 2017 by Jadhav.Pranit

Hi support team,

   I use IAR as IDE, and I have several boars on which there are several sensors, all controls by the the ADuCM3029. I have done several tests on different boards (which are all the same), and some of them work correctly, but the others, after several tests gives me the following error message  : "Failed to get CPU status after 4 retries".

So i have this error or not, depending of the board i use.

 

I use a J Link debuger, and I am in CPU debug.

 

The following is my Error LOG.

 

Mon Jul 31, 2017 13:43:49: Loaded macro file: C:\Program Files (x86)\IAR Systems\Embedded Workbench 7.2\arm\config\flashloader\AnalogDevices\FlashADUCM3029.mac
Mon Jul 31, 2017 13:43:50: JLINK command: ProjectFile = C:\Users\avouaill\Desktop\workspace\Puck_project_debug_Beacon_Juillet_2017\Puck_project\settings\second_test_Debug.jlink, return = 0
Mon Jul 31, 2017 13:43:50: Device "ADUCM3029" selected.
Mon Jul 31, 2017 13:43:50: DLL version: V6.10c, compiled Sep 28 2016 18:45:15
Mon Jul 31, 2017 13:43:50: Firmware: J-Link Lite-ADI Rev.1 compiled Jan  7 2013 17:58:04
Mon Jul 31, 2017 13:43:50: Selecting SWD as current target interface.
Mon Jul 31, 2017 13:43:50: JTAG speed is initially set to: 1000 kHz
Mon Jul 31, 2017 13:43:50: Hardware reset with strategy 3 was performed
Mon Jul 31, 2017 13:43:50: Initial reset was performed
Mon Jul 31, 2017 13:44:15: Fatal error:    Session aborted!
Mon Jul 31, 2017 13:44:15: Unloaded macro file: C:\Program Files (x86)\IAR Systems\Embedded Workbench 7.2\arm\config\flashloader\AnalogDevices\FlashADUCM3029.mac

 

Any idea to solve this let me know,

Thank by advance.

Outcomes