AnsweredAssumed Answered

will this AD-FMCMOTCON2-EBZ motor control design be suitable for 220V 7.5Kw PMSM if we customize the driver board?

Question asked by shalini.ice50@gmail.com on Jul 28, 2017
Latest reply on Jul 31, 2017 by ACozma

will this AD-FMCMOTCON2-EBZ motor control design be suitable for 220V 7.5Kw PMSM if we customize the driver board? The power MOSFET are rated for max 60V and suitable for driving 12-48V motors. For my motor rating, i want to know that if i replace MOSFET by power IGBT with little circuit corrections will I be able to use the same reference design( source code) given by analog device ..?

Outcomes