AnsweredAssumed Answered

ad9984a 720p60 not supported

Question asked by Abdulhadi on Jul 27, 2017
Latest reply on Jul 28, 2017 by Abdulhadi

Currently, I'm using the AD9984a to convert VGA signals to HDMI signals, the 1080p-60 configuration script seems to work in setting the output resolution to 1080p but all the other scripts result in black borders with distortions (including the 720p60 script when the VGA input is a 1280x720 signal) when output to a monitor.  Occasionally, the monitor after the configuration is changed also just freezes.  Any insight/help in debugging this issue is much appreciated. 

 

model: AD9984AKSTZ

Outcomes