AnsweredAssumed Answered

2 signals from FMCDAQ2?

Question asked by justinklchan on Jul 26, 2017
Latest reply on Jul 27, 2017 by andrei_g

The FMCDAQ2 has 2 outputs.

 

Does this mean I can transmit two completely different signals?

 

Or does this mean I can only transmit one signal, and the I and Q signals are sent to each of the two ports?

 

I'm trying to transmit a 100MHz on TX1 and a 200MHz tone on TX2, instead all I get from the output ports are two 100MHz tones in quadrature. What's going on.

Outcomes