AnsweredAssumed Answered

Program ADRV-DPD1

Question asked by ken.sallings on Jul 25, 2017
Latest reply on Jul 26, 2017 by Benetel_Brian

Hardware: 

  • ZC706 evaluation board
  • ADRV-DPD1
  • Signal Generator Providing 30.72 MHz to J13 with a power of -3.0dBm

 

Software:

  • TES 2.0.67

 

I am having a problem using the ADRV-DPD1.  When I try to program the device, the status bar moves about 20%, then it halts with two error messages.  When I first connected, the TES updated the files on the Zynq board and rebooted it.

 

I am completely stuck.  Does anyone have any suggestions?

 

Attached are two error screen shots, the error log, and the gui setup file.

Outcomes