AnsweredAssumed Answered

Setting Comparison frequency in HMC-C070

Question asked by kashef85 on Jul 25, 2017
Latest reply on Jul 27, 2017 by kashef85

Hi I want to use HMC-C070 Microsynth module with 100MHz REFin. The datasheet states that REFin input can be up to a maximum of 220MHz, however comparison frequency should be less than 75MHz.

Fref=Frefin/R.

I believe, i need to set the R value to prescale Reference signal. I was not able to find where to set the R value in the register map.

Outcomes