AnsweredAssumed Answered

ADSP-21469 EZ-Board DDR2 access issues

Question asked by ChristianH on Oct 20, 2011
Latest reply on Oct 21, 2011 by ChristianH

Hi,

 

I got a core hung (according to the VDSP error message) but I'm not sure what's the reason.

 

Following code fails

dm(m0,i0) = r3;                                            //m0 is 0x200000 (DDR2 start address), i0 is 0...2000000

 

but this one works.

modify(i0,m0);                                              //m0 is 0x200000 (DDR2 start address), i0 is 0...2000000
dm(i0,m5) = r3;                                            //m5 is 0x0

 

I've enabled the SIMD mode in the MODE1 register in both cases.

The code is inside an SPORT irq routine.

 

In both cases I would expect that r3 is stored to address (i0+m0) and s3 is stored to address (i0+m0+1).

 

Regards

Christian

Outcomes