AnsweredAssumed Answered

On the selection of AD9106 and AD9959

Question asked by 1053804627 on Jul 24, 2017
Latest reply on Jul 27, 2017 by Biao.H

Both the AD9106 and AD9959 chips use DDS technology and can be used as the signal generator of the sinusoidal wave signal. How to select the two chips?Why is that?I hope that experts can give you some answers.Going to do (one output of the phase difference of 120 ° 3 sinusoidal ac signal source, frequency is 500 hz, amplitude, frequency, phase difference can be programmed to modify Settings)

Outcomes