AnsweredAssumed Answered

Hi, i would like to cascade two amplifiers together. The first stage will be the HMC465LP5 and the second stage will be the HMC994APM5E. I am planning to create a layout with 50ohm lines connecting these two on Rogers 4350B PCB. Is there anything I should

Question asked by mmbiedka on Jul 24, 2017
Latest reply on Aug 2, 2017 by SMcBride

I want to make sure that all I need to do is connect the output of the HMC465LP5 to the input of the HMC994APM5E through 50 ohm line.

Outcomes