AnsweredAssumed Answered

Using AD829 as a low-pass filter

Question asked by lt0337 on Jul 22, 2017
Latest reply on Aug 4, 2017 by leandro_pj

Hello, I want to use AD829 as a low-pass filter, dose it work stable in the following conditions?

- Clead=100pF capacitor

- R2=~2kohms resistor load

-Gain=4

- Vs = +/- 5V

- Ccomp = 7pF to ground

The circuit schematic is same as figure 36 in datasheet of AD829

And dose the Slew Rate or noise gain or other paremeters of the circuit change by increasing the value of Clead?

 

Thanks for your answer.

Outcomes