AnsweredAssumed Answered

AD9373 Profile Configuration

Question asked by jyothibasu on Jul 18, 2017
Latest reply on Jul 21, 2017 by sripad

we are using the Linex source code from ADI to configure the TRX.

i found there is some Default configuration in the code. 

we tryed to configure the Profile as attached and it gives "ARM configuration error 432"

is there any other parameters need to modify, we did changes to all Profiles TX/RX/ORX/SRX still same issue.

 

if we use 307.2MHz Devise clock/TX sampling 307.2MHz/ORX 153.6MHz:

what is the TX DAC Filter 3dB Corner?? what will be the number

what is the BBF 3dB Corner?? what will be the number

Attachments

Outcomes