AnsweredAssumed Answered

Can I change the frequency of the square wave output in a AD9837?

Question asked by nm_eng17 on Jul 18, 2017
Latest reply on Jul 19, 2017 by nm_eng17

Can I change the frequency of the square wave output in a AD9837?

 

I have it set to generate a square wave with the DAC disabled. After I set a value in the freq0 register and re-enable the device, the output frequency is always 78KHz, regardless of the value programmed into the freq0 register. 

 

The input clock is 5MHz. 

Outcomes