AnsweredAssumed Answered

AD9889B video do not output on the HDMI

Question asked by Lodge on Oct 19, 2011
Latest reply on Oct 28, 2011 by cvaughn

Dear all,

input source is a 1280x720p  4:2:2 (Y'C'BC'R) 10-bit  video. I had test ad9889's pin6 clock rate is 148.5 MHz。

And ad9889 has detected the source format.

 

here is the read back i2c value,

 

0x0    0  0  0  0  4  42 80 0  0  0  0  26 3C 18 1  13
0x10 25 37 0  0  0  6  D6 2  6  62 4  A8 0  0  1C 84
0x20 1C BF 4  A8 1E 70 2  1E 0  0  4  A8 8  12 1B AC
0x30 0  0  0  0  0  0  0  0  0  0  0  80 0  13 4C 0 
0x40 0  10 E0 7E 78 98 48 80 0  0  0  0  0  0  0  0 
0x50 0  0  0  0  0  0  0  0  0  0  0  0  0  0  0  0 
0x60 0  0  0  0  0  0  0  0  0  0  0  0  0  0  0  0 
0x70 0  0  0  0  0  0  0  0  0  0  0  0  0  0  0  0 
0x80 0  0  0  0  0  0  0  0  0  0  0  0  0  0  0  0 
0x90 0  0  0  0  C0 0  34 0  7  2  0  18 38 61 12 70
0xA0 0  0  84 84 0  0  0  0  0  0  0  0  0  0  40 2 
0xB0 94 BA 91 9F CA D5 D8 43 10 0  0  FF 0  0  0  0 
0xC0 0  0  0  0  0  10 4  0  2  3  0  1  2  0  0 

 

What's wrong on it ?

Outcomes