AnsweredAssumed Answered

AD4667R out of spec

Question asked by valerionew on Jul 17, 2017
Latest reply on Aug 3, 2017 by isantos

Hi, 

for me it's the first time using analog devices products. I've asked and received a sample of the AD4667R DAC

Yesterday i've started to write the code for it. After a while i realize that the output that the dac is giving is 500mV over the setting. For example, with all zeros loaded into the dac i read about 500mV on the output. So i've measured Vref out and i measure about 3V instead of 2.5V that the datasheet says. 
Why is it so out of spec? 

Outcomes