AnsweredAssumed Answered

What is the output rate of the ad9371 ip core for TX?

Question asked by arodgers234 on Jul 14, 2017
Latest reply on Jul 24, 2017 by AdrianC

I'm somewhat confused as to what the clock rate is for the 9371. I have a profile generated to run my evaluation board at 100 MHz, however, the profile lists a clock rate of over 200 MHz. My understanding is that this is oversampled so that some additional processing can be done in the Ad9371.

 

My question is what this means for the PL logic. There is a 16 bit output on the AD9371 IP core for each I and Q of each Rx chain(and similarly one for the AD9361). Is the output rate of this IP block 200 MHz or higher than this?

Outcomes