AnsweredAssumed Answered

How do I configure the AD9361 for 2R1T using default_init_params.h?

Question asked by StevieK on Jul 13, 2017
Latest reply on Jul 28, 2017 by StevieK

How do I configure the AD9361 for 2R1T operation using default_init_params.h? If I set two_rx_two_tx_mode_enable=1, it looks like the driver software will enable both Tx channels (2R2T), which I don't want. If I leave that at zero but set two_t_two_r_timing_enable=1, it doesn't look like the driver software uses that parameter in setting the data_clk frequency. Is there a better solution than setting two_rx_two_tx_mode_enable and then having to manually disable Tx2?

Outcomes