AnsweredAssumed Answered

AD8655 parameters modeled?

Question asked by industrieel on Jul 13, 2017

Hi, 

 

I'm using ADIsimPE to model a circuit built around the AD8655 op-amp. Particularly I want to know if the model takes into account the input capacitance and input resistance of the device.

 

From the application note, I understood that the models provided by AD are encrypted. In the installation directory I believe to have found the models, which indeed are (except for a "header" file per device) not readable. The directory I'm referring to is  'C:\Program Files (x86)\ADIsimPE_800\support\models\analog_devices_linear_encrypted.lb'. 

 

This file contains a field (in the header) for the AD8655 called "Parameters modeled include:", but the field is not filled in. Hence, I can not derive from this whether the model includes the input capacitance and/or input resistance.

 

Could someone help me with finding this information?

 

 

Kind regards,

Industrieel

Outcomes