AnsweredAssumed Answered

ADP7118 PSRR and noise graph for 15V output.

Question asked by alperen on Jul 12, 2017
Latest reply on Jul 24, 2017 by AIlustrisimo

Hello,

I am planning to use ADP7118 to regulate my switching regulator's output. The output voltage of ADP7118 is going to be 15 with 0.5V to 1V headroom and the load is about 80mA to 120mA. I need PSRR and noise spectrum graph under these conditions. I am unable to find such information in the datasheet of ADP7118.

Thanks in advance.

Outcomes