AnsweredAssumed Answered

Use of ADV7125 as a general DAC

Question asked by BCAO on Jul 7, 2017
Latest reply on Aug 3, 2017 by edo

Use of ADV7125

1. Can the three RGB (six differential) outputs of controlled independently if sync_n = 0 and blank_n = 1? I this case, are the RGB outputs true differential?

2. Can this device drive single terminated 50 ohm loads?

3. Is it truly 330 MSPS?

4. What is the op-amp to convert the differential current outputs to single-ended voltage outputs?

5. Does the clock input need 50 ohm impedance matching?

Outcomes