AnsweredAssumed Answered

Help with PPI Example for BF592 EZ-Kit Lite

Question asked by rbrt on Oct 17, 2011
Latest reply on Oct 18, 2011 by Prashant

Hi,

 

I'm trying to run the PPI example for the BF592 EZ-Kit Lite. I have followed the instructions in the readme file, but would appreciate some clarification on a couple of points:

 

- When setting up the clock, the readme states to connect a lead from "lead from interface  P4 31 (PF11) to interface P6 16 (PPI0CLK)". I have connected a lead between Pin 31 of P4 and Pin 16 of P6. However, in the reference schematic, P6, 16 is labeled PPI0CLK, but P4, 31 is labeled UARTTX rather than PF11. Did I connect the proper pins together?

 

- Which Pin(s) of P6 do I need to access to observe the PPI data activity?

 

Thanks for any help!

Outcomes