AnsweredAssumed Answered

ADD5211 power on

Question asked by AD-Sven on Jul 3, 2017
Latest reply on Jul 6, 2017 by AD-Sven

Dear Sir/Madam,

I`m using the ADD5211 to drive a LCD backlight, but sometimes (very rare) it doesn´t power on.

After connecting the EN-pin or the UVLO-pin shortly to ground it starts again.

Unfortunately I didn´t connect the Fault-pin, so I can`t monitor any fault state.

I tried to connect EN-pin or UVLO-pin via a 100kOhm resistor to VIN, but without any success.

 

I can also reproduce it by permanent powering the ADD5211 and switching off/on the EN-pin.

 

I already ordered the evaluation board and use quite the same values for all components,

but could not reproduce the faulty behavior.

 

Production date ADD5211: 1319 @ADD5211-Evalboard and 1634 in my design

 

Any idea?

 

Many thanks,

Sven

Outcomes