AnsweredAssumed Answered

ADV7611's I2C programming example Request

Question asked by Sercan on Jul 3, 2017
Latest reply on Jul 3, 2017 by JeyasudhaMuthuPerumal

Hi,

 

In order to get HDMI output from the ADV7511,

  * I am using the I2C_Sender module given at the below link. You can also find this module's vdhl code at the attachments.

        Zedboard HDMI v2 - Hamsterworks Wiki! 

  * Where there is a 100 MHz clock-in and where module programs the Adv7511.

 

I am making an HDMI IN/OUT project which will insert some basic drawings to the HDMI-In and will give HDMI-Out from an ADV7611.

At this project i am using ZedBoard (that has ADV7511) and Digilent's FMC-HDMI Daughter Card (that has ADV7611).

 

 

I don't have enough time to study & learn the I2C programming in details.

So, does any one can offer me how to program ADV7611?

 

--- OR

If I design a programmer module like adv7511 example I mentioned,

I see,

I have to use ADV7611 addresses as 98, 68 and so on?

 

Is there a limitaion like "after changing address from 98 to 68 for example, do i have to wait for a while?"

And can you please inform me about the critical points about the "ADV7611's I2C_Programmer module design" issue? 

 

Best regards,

& Sorry for my lazy-to-research,

Sercan

Attachments

Outcomes