AnsweredAssumed Answered

broken? make for "hdl_2016_r2" project "pzsdr1.ccbrk_cmos"

Question asked by Gastraea on Jul 3, 2017
Latest reply on Jul 5, 2017 by CsomI

Hi all

I have an AVNET picozed sdr 1x1 SOM with the PicoZed SDR Breakout Carrier
I have been trying to create the project files for this from the git repo. I tried hdl_2016_r1 but that seem to be set up for sdr2 so I changed to hdl_2016_r2. As this is pre-release there may be bugs.

 

I am using Vivado 2016.2, Win 10, cygwin64 and downloading the repo as a zip.

in the base directory I am running 

 

make pzsdr1.ccbrk_cmos

 

all goes well till it hits the following error.

 

.....................

### create_bd_port -dir I tdd_sync_i
### create_bd_port -dir O tdd_sync_t
ERROR: [BD 5-216] VLNV <analog.com:user:axi_ad9361:1.0> is not supported for the current part.
ERROR: [Common 17-39] 'create_bd_cell' failed due to earlier errors.

while executing
"create_bd_cell -type ip -vlnv analog.com:user:axi_ad9361:1.0 axi_ad9361"
invoked from within
"set axi_ad9361 [create_bd_cell -type ip -vlnv analog.com:user:axi_ad9361:1.0 axi_ad9361]"
(file "../common/pzsdr1_bd.tcl" line 204)

while executing
"source ../common/pzsdr1_bd.tcl"
(file "system_bd.tcl" line 2)

while executing
"source system_bd.tcl"
(procedure "adi_project_create" line 98)
invoked from within
"adi_project_create pzsdr1_ccbrk_cmos"
(file "system_project.tcl" line 7)
INFO: [Common 17-206] Exiting Vivado at Mon Jul 03 08:06:25 2017...

 

Am I doing something wrong?

 

Thanks

Outcomes