AnsweredAssumed Answered

HMC7044 Bidirectional Signals Interface

Question asked by donaldt on Jun 27, 2017
Latest reply on Jun 27, 2017 by pkern

Good day,

I need to connect the digital bidirectional pins of the HMC7044 to a component via a voltage level translator.
Thus I need a device that can provide signal levels that satisfies the input requirements of the HMC7044:
  V_IH > 1.22 V
  V_IL < 0.24 V

The device should be able to accept these output signal levels from the HMC7044:
  1.6 < V_OH < 2.2
  V_OL < 0.1

The device needs to translate the signal levels to LVCMOS18.

Does Analog Devices provide a component for this application?

Outcomes