AnsweredAssumed Answered

Using AD6688/AD9208 in Sub-class 0 Mode

Question asked by spraju87 on Jun 27, 2017
Latest reply on Jun 28, 2017 by UmeshJ

Hello, 

 

As we do not require deterministic latency for our application (spectrum analyzer), we are planning to set-up the JESD204B interface between the ADC and FPGA in sub-class 0 mode. We use Xilinx Kintex ultrascale FPGA for base-band processing. Also, the ADC configuration/sampling rate is such that, the lane rates can be as high as 12.5 Gbps

 

Although, the data sheet of the ADCs and Xilinx JESD IP core say that sub-class 0 mode is supported, I would like to confirm the following :

1) Does operating the JESD204B in sub-class 0 mode have any side effects that we should be aware of ?

2) Does it affect the lane rate in any way ?

3) Can I leave the SYSREF pins floating if I only need sub-class 0 operation ? (the data sheet says so)

4) Since AD6688/AD9208 have dual ADC cores, does not having SYSREF cause any issues in the alignment of samples between these two ADC cores on the Rx side (FPGA) ?

 

Thanks,

Raju

Outcomes