AnsweredAssumed Answered

On the EVAL-AD5292EVB, what is the resistance value (RAB = 20K, 50K or 100K) on the version of the AD5292 used on this board; i.e. what is the part suffix?

Question asked by curtg Employee on Jun 26, 2017
Latest reply on Jun 26, 2017 by rrosario

Could you provide the full part number for the AD5292 used on the EVAL-AD5292EBZ? If the AD5292-100 is used and one wants to evaluate the AD5292-20, what do you recommend? Does one have to remove the AD9252 from the board and replace it with the version that one wants to evaluate?

Attachments

Outcomes