AnsweredAssumed Answered

ADV8005 TX without input signal

Question asked by Fermat on Jun 22, 2017
Latest reply on Jun 28, 2017 by Fermat

Dears

 

I have a question about ADV8005 TX,

 

My setting is Use PrimaryVSP and Tx1, and OSD and SecondaryVSP and RX are disable. 

 

Video TTL Input[No Signal] --> Primary VSP --> Tx

 

Can ADV8005 Tx output 1080P or any timing without no input signal?

 

[No input signal]  --> Primary VSP --> Tx1 ?

 

 

 

Is it possible? freeRun mode? or any setting?

 

Because I have another process after ADV8005, I want to confirm if ADV8005 can output default timing before there is signal input.

 

Thanks

Ken

Outcomes