AnsweredAssumed Answered

ADP5350 with JEITA SPEC

Question asked by Mochi on Jun 21, 2017
Latest reply on Sep 1, 2017 by Mochi
It is a question when using ADP5350 with JEITA SPEC.
In setting up according to JEITA SPEC, the temperature of table 13 of the data sheet was guaranteed.
For example, when the temperature rises from the area of JEITA_COLD (0 ° C or less), what is the hysteresis width that switches to the area of JEITA_COOL (0 ° C min / 10 ° C max)?

Best regards

Outcomes